This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050EVM-561: Question about operation of the BQ4050EVM

Part Number: BQ4050EVM-561
Other Parts Discussed in Thread: BQ4050, BQSTUDIO

Hi

Inquire about the operation of the BQ4050.

It is operating as follows.

- Current voltage: 13.2 volts (battery voltage)
- Discharge voltage: 0V (keep cut off)
- During charging: Charging to 2A is normal

problem
a. When discharging, the voltage is not output and remains shut off, and when the Wake Switch is pressed, the voltage is output only while it is pressed.
b. It should automatically wake up when charging, but it only lasts for a while when charging, and drops to 0V as soon as charging stops (maintain blocking)

Thanks