TPS65987D USB Type-C® and USB PD Controller with Integrated Source and Sink Power Path Supporting USB3 and Alternate Mode (TPS65987D SLVSES1D – MAY 2018 – REVISED OCTOBER 2022)
Questions(1)
8.3.5 Dead Battery Operation
8.3.5.1 Dead Battery Advertisement
The TPS65987D supports booting from no-battery or dead-battery conditions by receiving power from VBUS.
Does "booting from no-battery or dead-battery conditions" refer to the TPS65987D without the "VIN_3V3" input?
Or do you mean that the system (host side) that implements the TPS65987D does not have a power supply to charge the external device?
Questions(2)
8.4 Device Functional Modes
8.4.1 Boot
At initial power on the device goes through a boot routine. This routine is responsible for initializing device register values and loading device patch and configuration bundles. The device's functional behavior after boot can be configured through the use of pin straps on the SPI_POCI and ADCIN1 pins as shown in Table 8-5.“
In our system, if "The TPS65987D do not load any ROM patch and-or configuration from flash memory during the boot sequence."
Will the state of TPS65987D after “a boot routine” be as described in Table 8-5?