This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150: Please help check the schematic diagram, thank you

Part Number: TPS65150

Dear TI

       Please help check the schematic diagram, thank you.

       input: 5V

       output:   

                 AVDD: 8.2v      max 120mA

                VGH: 12.5V      max 1mA

                VGL: -13V         max 1mA