I've the bq2002t with TM=0 and ten cells.
It seems function but after 40 minutes the device go out from the fast charge state
and go in the top-off state. I put the thermistor in air, not in the pack and I restarted the
charge cycle. After few minutes the device go in top-off. So the temperature doesn't affect this changing.
The only reason is the negative delta voltage.
I tested 2 different battery pack (2100mA) with same results.
So the battery pack is far to being charged. 700mAh are missing...
Could the top-off state complete them?
Is a normal behaviour?
What do you say me?
Bye