Hi,
I want to know is there any way to decrease the reaction time when protection is happening? BQ25731 is working on OTG mode. Input voltage is 7V and output voltage is 3.5V. Blue line is the output voltage, yellow line is the inductor voltage, purple line is the driver signal. the total time is 16.5ms from that the output voltage starts to oscillate until it drop to zero.