This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: GPCCEDV: CEDV coefficients EDVR0 from GPC report out of bqstudio's value range?

Part Number: BQ4050
Other Parts Discussed in Thread: BQSTUDIO, BQ78350-R1, GPCCEDV

Hi,

I have received the GPC report for the discharge logs of a BQ4050 CEDV Gas Gauge with two Lithium Ion (LG INR18650-MJ1 3500mAh) cells placed in series. The CEDV parameters from the report read as follows:

EMF    5968    
EDVC0    101    
EDVC1    0    
EDVR1    1    
EDVR0    128143    
EDVT0    4452    
EDVTC    11    
VOC75    7871    
VOC50    7617    
VOC25    7504

I entered the parameters in bqstudio but got an error for EDVR0 after trying to enter 128143 in the R0 field under (Gas Gauging --> CEDV cfg):

"Value is beyond maximum value defined for parameter."

I have checked the TRM (https://www.ti.com/lit/ug/sluuaq3a/sluuaq3a.pdf?ts=1693811569270) and the maximum value allowed for R0 is 65535.

I'm wondering if I'm interpreting the CEDV parameters from the report correctly (like suggested here for the BQ78350-R1 gauge: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/763132/bq78350-r1-capacity-learning/2820936?tisearch=e2e-sitesearch&keymatch=edvr0%2520r0#2820936)

EMF         -->    EMF
EDVC0    -->    C0 
EDVC1    -->    C1
EDVR1    -->    R1
EDVR0    -->    R0   
EDVT0    -->    T0
EDVTC    -->    TC

The TRM also states (section 6.4.1):

"R0 is the first order rate dependency factor stored in EDV R0 Factor/EDV2."

I'm not using a fixed EDV2 in my configuration (EDV_CMP=1). If above formula is correct, how can I determine the dynamically calculated EDV2?

Thank you in advance.

Tom