Hi team,
Is the customer in the project? Due to a manufacturing error, the three-way connection between the light string and the chip OUT (OUT1/OUT2/OUT3) was mistakenly connected together in the connector design. As shown below:
From my personal understanding, it is not very reliable to connect three light string signals with different phases in parallel. I would like to ask what impact such wrong connection will have on the function of LP8860? Is there a risk?