This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: PIN 15 config not matching SLUUBT5C

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO

Hello,

Based on the above config,

PIN 15 should be GPIO. But my DISP function is activated by above config. 0,1 bits don't enable DISP function. 

Can someone verify my pin config with below?

PIN12: TS3

PIN13: TS4

PIN15: DISP

PIN16: PDSG

PIN17: PRES

Thank you! 

  • Hi Saero,

    PIN12: 001, TS3

    PIN13: 001, TS4

    PIN15: 01, DISP

    PIN16: 01, PDSG

    PIN17: 000, PRES

    Verified using the BQ40Z80 Technical Reference Manual found below:

    https://www.ti.com/lit/pdf/sluubt5 

    Regards,

    Anthony Baldino

  • My mistake, PIN15 is actually 10 which is GPIO.

    Regards,

    Anthony Baldino

  • Yes. This is what I expected. But with this config, my PIN15 is working as DISP. 

    Is there a way to check whether there's a bug or documentation error?

    Thank you. 

  • Hi Saero,

    In the Technical Reference Manual, the description of the Pin Configuration is stated as so:

    I believe that this caused our issue, since it reads SEL0, SEL1 when in bqStudio it reads SEL1, SEL0.

    In the screenshot you have above, you have it set as 01, which is DISP. I would flip those options and try it.

    Sorry about the confusing documentation.

    Regards,

    Anthony Baldino

  • Hello, 

    I tried flipping the option. It works only with above attached picture config.

    Thank you!

  • Hi Saero,

    Have you tried resetting the gauge since making those changes? The gauge will not implement changes unless reset.

    Regards,

    Anthony Baldino

  • Hello,

    Yes, I have reset gauge after parameter change. 

    I was using pin13 for DISP before. I shifted to PIN15 and seems to work in opposite condition to documentation. 

    Please check the log below with srec file.
    I have trigger DISP twice in log.

    drive.google.com/.../view

     

    Fri Sep 08 20:25:43 IST 2023
    
    Device Version Info = 4800_0_04
    BQZ Device Name = bq40z80
    BQZ Firmware Version = V0_04_BLD5
    
    Design Capacity = 6000
    Design Voltage = 22200
    Specification Info = 0x0031
    Manufacturer Date = 1980-1-1
    Serial Number = 0x0001
    Manufacturer Name = Texas Instruments
    Device Name = bq40z80
    Device Chemistry = LION
    
    Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellCurr5,CellCurr6,CellCurr7,CellPower1,CellPower2,CellPower3,CellPower4,CellPower5,CellPower6,CellPower7,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,RaScale5,RaScale6,RaScale7,CompRes1,CompRes2,CompRes3,CompRes4,CompRes5,CompRes6,CompRes7,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,CellGrid5,CellGrid6,CellGrid7,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0_5,DOD0_6,DOD0_7,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,DODEOC_5,DODEOC_6,DODEOC_7,QMax1,QMax2,QMax3,QMax4,QMax5,QMax6,QMax7,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxDOD0_5,QMaxDOD0_6,QMaxDOD0_7,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,RawDOD_5,RawDOD_6,RawDOD_7,CBTime1,CBTime2,CBTime3,CBTime4,CBTime5,CBTime6,CBTime7,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBDOD_5,CBDOD_6,CBDOD_7,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
    1,2023-09-08 20:25:45,2.007,0x0187,300,10,0x6001,0,65535,65535,1,27.4,23062,0,0,1,63,49,2915,4694,65535,65535,65535,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3840,3823,3830,3842,3848,0,23001,22996,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.5,27.3,27.8,-273.2,-273.2,27.3,27.8,27.3,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,259,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1146,SUCCESS
    2,2023-09-08 20:25:47,4.077,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23063,0,0,1,63,49,2915,4694,65535,65535,65535,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3840,3823,3830,3842,3848,0,23002,22996,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,26.4,27.3,27.8,-273.2,-273.2,27.2,27.8,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,261,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1201,SUCCESS
    3,2023-09-08 20:25:49,6.018,0x0187,300,10,0x6001,0,65535,65535,1,27.3,23062,0,0,1,63,49,2915,4694,65535,65535,65535,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3841,3823,3830,3843,3848,0,23028,23020,22,27,22,24,-5,-6,0,9,10,8,9,-2,-2,0,9,0,27.3,27.4,27.8,-273.2,-273.2,27.4,27.8,27.4,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,263,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1180,SUCCESS
    4,2023-09-08 20:25:51,8.092,0x0187,300,10,0x6001,0,65535,65535,1,27.3,23065,12,1,1,63,49,2915,4694,65535,65535,65535,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0002,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3841,3823,3830,3843,3848,0,23029,23021,19,19,20,6,-10,-7,0,7,7,8,2,-4,-3,0,21,2,28.2,27.2,27.8,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,265,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1221,SUCCESS
    5,2023-09-08 20:25:53,10.029,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23064,9,2,1,63,49,2915,4694,65535,65535,53370,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0002,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3841,3823,3830,3842,3848,0,23004,22998,11,6,21,16,-14,-11,0,4,2,8,6,-5,-4,0,18,5,28.5,27.2,27.7,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,267,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1155,SUCCESS
    6,2023-09-08 20:25:56,12.117,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23063,0,2,1,63,49,2915,4694,65535,65535,53370,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3840,3823,3829,3842,3848,0,23000,22996,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5,26.9,27.2,27.8,-273.2,-273.2,27.2,27.8,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,269,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1193,SUCCESS
    7,2023-09-08 20:25:57,14.035,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23061,0,2,1,63,49,2915,4694,65535,65535,53370,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3841,3823,3830,3842,3848,0,23001,22996,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,4,26.8,27.2,27.8,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,271,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1165,SUCCESS
    8,2023-09-08 20:26:00,16.108,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23063,0,2,1,63,49,2915,4694,65535,65535,53370,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3841,3823,3830,3842,3848,0,23001,22996,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,4,26.6,27.2,27.8,-273.2,-273.2,27.2,27.8,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,273,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1171,SUCCESS
    9,2023-09-08 20:26:01,18.044,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23061,4,1,1,63,49,2915,4694,65535,65535,65535,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0002,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3841,3824,3830,3843,3848,0,23024,23021,12,20,23,12,-6,-4,0,5,8,9,5,-2,-2,0,16,3,27.9,27.2,27.7,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,275,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1189,SUCCESS
    10,2023-09-08 20:26:04,20.109,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23065,9,3,1,63,49,2915,4694,65535,65535,35580,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0002,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3840,3824,3830,3843,3848,0,23021,23018,19,29,24,22,-7,-6,0,7,11,9,8,-3,-2,0,23,6,28.4,27.2,27.7,-273.2,-273.2,27.2,27.6,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,277,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1187,SUCCESS
    11,2023-09-08 20:26:05,22.063,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23064,7,3,1,63,49,2915,4694,65535,65535,35580,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3841,3823,3830,3842,3848,0,23001,22995,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,8,27.7,27.2,27.7,-273.2,-273.2,27.1,27.7,27.1,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,279,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1150,SUCCESS
    12,2023-09-08 20:26:08,24.106,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23063,0,3,1,63,49,2915,4694,65535,65535,35580,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3880,3841,3823,3830,3842,3849,0,23002,22995,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,7,26.9,27.2,27.7,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,281,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1142,SUCCESS
    13,2023-09-08 20:26:09,26.070,0x0187,300,10,0x6001,0,65535,65535,1,27.2,23062,0,3,1,63,49,2915,4694,65535,65535,35580,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3841,3823,3830,3842,3848,0,23002,22995,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,6,26.8,27.2,27.7,-273.2,-273.2,27.2,27.7,27.2,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,283,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1191,SUCCESS
    14,2023-09-08 20:26:12,28.131,0x0187,300,10,0x6001,0,65535,65535,1,27.1,23064,0,2,1,63,49,2915,4694,65535,65535,53370,4200,25200,0x00C0,1,-32767,-25738,-24000,-12000,93,0x0187,0x0000,0x10,0x0004,0x50,0x0014,0x0218,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3879,3840,3823,3830,3843,3848,0,23002,22995,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5,26.7,27.2,27.7,-273.2,-273.2,27.1,27.7,27.1,2915,6043,4694,10287,3526,2915,6043,1779,4244,4694,10287,26.7,26.6,1000,1000,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,6,0,0,0,0,0,0,0,285,5616,6160,6368,6288,6120,6064,0,0,0,1,560,0,88,0,0,0,0,5765,5844,5768,5813,5834,5848,0,0,0,0,0,0,0,0,0,1,1.83,252,5616,6160,6368,6288,6120,6064,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,5568,12268,1194,SUCCESS
    

  • Hi Saero,

    Is there a possibility you can send the .gg file you have for the gauge?

    Regards,

    Anthony Baldino

  • Hello,

    Please find .gg file below. Thank you!

    HG2.gg.csv

  • Hi Saero,

    Thank you for sending. I will attempt to recreate your issue and get back to you by the end of the week.

    Regards,

    Anthony Baldino

  • Hi Saero,

    Can you tell me which version of the firmware of bq40z80 you are using?

    Regards,

    Anthony Baldino

  • Hello,

    I'm on v0.04.

    Latest one I could find. Were you able to reproduce? My TS3 temperature works when I invert it similar to DISP. 

    Thank you! 

  • Hi Saero,

    I have not been able to reproduce the error yet. Using the bq40z80 EVM, the .gg file you sent correctly sends a GPIO signal out of pin 15. Still looking into other aspects that might have created this error.

    Regards, 

    Anthony Baldino

  • Hi Saero,

    I have placed a request with the firmware team to see if this is a firmware issue. I will keep you updated when I get a response.

    Regards,

    Anthony Baldino

  • Hello,

    awaiting response. 

    Thank you!

  • Hi Saero,

    Still have not gotten a response yet. Will reach back out to them and try to have an update for you by the end of tomorrow.

    Regards,

    Anthony Baldino

  • Hi Saero,

    Please try updating the devices firmware to the latest version found below and let me know if the issue still occurs:

    https://www.ti.com/product/BQ40Z80 

    Regards,

    Anthony Baldino

  • Hello, 

    I'm already on latest firmware. Was there any release recently??

    Thankyou 

  • Hi Saero,

    I was informed by the firmware team that the v0.04 firmware is not the most recent version. The current v1.0 firmware is the most recent and can be found on the product page for bq40z80.

    Regards,

    Anthony Baldino

  • Hello,

    I don't think so. At least not available from the link shared. v0.04_build_5 is the latest.

  • Hi Saero,

    Just confirmed with the firmware team that the newer versions are still in the process of getting cleared to be released to the public.

    In the mean time, can you share the schematic you are using for this device?

    Regards,

    Anthony Baldino