This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: TI's battery charger IC solution

Guru 12655 points
Part Number: BQ25756
Other Parts Discussed in Thread: BQ25155, BQ25798

Hi, 

Are there any applicable products for TI's battery charger?

Requirements:
・Lithium polymer battery 1 cell
・Input voltage max: 8V or higher
・Charging voltage: 4.2V
・Battery temperature monitoring function
・Over-charge and over-discharge protection
・Charging current monitoring function
・Voltage remaining monitor function

Prerequisites:
Charging current (at CC): 100mA or more
With LDO: 2V to 3V

We have set the remaining battery level monitor function and charge current monitor function as requirements, However, if it is too difficult to build in the battery charger, we would like to know about external components.

Thanks,

Conor