This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Iso. Sw. Reg. Design Consultant

I am looking for two isolated switching regulator designs:

First one:

With 48V in, I want a programmable output range of 19V to 29V at 8A

With 36V in, I want a programmable output range of 10V to 16V at 8A

 

Second one:

With 36V in, I want a programmable output range of -10V to -19V at 9A

With 24V in, I want a programmable output range of -4V to -10V at 9A

 

For both, I want >90% efficiency when the output power is near its maximum.

The programming could be digital or analog but need not be accurate (we measure the output voltage and can trim the programming accordingly).

Is there anybody out there who can do such designs readily or point me to existing products that would do the job? 

  • Hello John,I am Neil Pattison and I design all types of power supplies.I am based in Adelaide,South Australia.I can do a design for you which would easily meet your efficiency requirements.Do you need only the schematic or do you require me to build it too?My charges are not extreme,as I am now retired and do not need to support a fully functioning business.Let me know your thoughts.Regards,Neil.