This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79600EVM: Doubt in BQ79600_UART_Sample_code

Part Number: BQ79600EVM
Other Parts Discussed in Thread: BQ79616, TMS570LS0714, BQ79600-Q1, USB2ANY

In the BQ79600_UART_Sample_Code:

  1. It is written there in the sample code comment (bq79616.h, line no 33), that it is incomplete, does not work right now (in first screenshot), so please clarify this how it will work.
  2. In this sample code TMS570LS1244 is used, for our application we are using TMS570LS0714. So, this code will work for it as well?
  3. In this code Response_ frame is also used, can we get little more details regarding the same?