Hi,
I have a USB C sink that I only want to request 20V @5A and I want to reject all other PDOs (by going back to 5V).
I have set two PDOs in advanced settings: Just 5V and 20V, however when I plug in a source that can only provide up to 9V, I am seeing 9V on PPHV.
I want to only request 20V@5A, I want to reject 20V@3A because the produce will consume more than 60W which will overpower the charger.
What do I need to do to make this happen?