Other Parts Discussed in Thread: TPS22914
Hi,
I want to design a circuit for battery charge and solid switch for system turn on/off,
1. when without USB_5V, than user use solid switch to on/off system.
2. when solid switch off, and user plugin USB_5V, than there has a charging current(4.2V/45mA) from V_system and through Load switch Vout to Vin and to Battery positive terminal.
The design purpose is for even solid switch =off , user sitll can through load switch to charge product.
My question as below:
1. Due to TP22916 has always on reverse current blocking function, is mean V_system current can't through Vout to Vin? If the answer is yes, is mean when i change Vout and Vin direction can solve this issue?
Note: when USB_5V exist , only has charge function , system other funtion will disable.
2. Is possible to use TPS22914B also? VIN connect to battery positive and Vout connect to V_system, when USB 5V plugin, through 22914 internal mos body diode to charge battery, but there has a concern point, if the battery protector is lock mode(sys gnd and battery gnd disconnection), it's mean VIN(battery+)=floating, in this situation, if EN=5V ; VIN=Floating, the MOS body diode still can work?
Thank you
BR
Andy