Other Parts Discussed in Thread: TPS62811-Q1, TPS628501
Hi,
We are using the TPS54719RTER buck converter for 1.8V and 1V for our application having two FPGAs (XC7S50-1FGGA484C, Spartan-7 series ).
Following is the requirement,
For 1V
Vin - 5V
Vout - 1V
Iout - 200mA (Static load)
total load capacitance - 120uF (decoupling capacitors)
For 1.8V
Vin - 5V
Vout - 1.8V
Iout - 200mA (Static load)
total load capacitance - 540uF (decoupling capacitors)
We need to know the how much inrush current will drive through the Input supply and whether it is reliable solution, possibly share waveform for the same.
We simulated the above requirement in Webench but could not able to find to simulate with adding capacitive load and with dynamic load.
For reference, attach the circuit.
Thanks.