Good day sir or madam,
Im currently testing the BQ25792. I have build a 4x4cm testing PCB following the guidelines in the BQ25792 datasheet with the same Inductivity as the EVM. Power is supplied by a external 300W power adapter. When discharging, I discharge with around 2.7A from a 10Ah battery with Max-discharge-current 5A. I now run into two problems that I just do not understand. Im hoping you could help me:
1) The way I understand Vsysmin is that Vsys is kept at Vsysmin (default 3.5V) as long as possible. If that is not possible anymore, the BQ25792 switches off the System voltage. Do I understand that correctly? Because Vsys In my tests always follows Vbat. Even when Vbat is below 3.5V it is still discharging until Vbat=2.8V, where the batteries PCM stops the charging. Even the lifted Vsys (compared to Vbat) that is mentioned in the NVDC part of the datasheet I do not notice. VSys mostly equals Vbat.
2) Our battery is supposed to be loaded with 5A. Setting the charge current up to 4A works fine. However setting it to 4.5A (with a supplied VBUS= 15V and IBUS_max=5A) makes the input current IBUS slowly break down. Looking into Register 33h confirms, that the charge current never reaches 4.5 A, but rather decrements slowly to around 3A. Register 03 still contains my input of 01C2h (for 450). Battery voltage according to 3Bh is around 3.7V, which I confirmed by multimeter. No fault is displayed. Even when decreasing the charge current now to something like 4A (03h->0190h) the current keeps dropping. I can not make sense of this behaviour. Do you have an idea what is going on and could help?
Thanks and regards,
Oliver BRedow