Hi i'm Nicola.
Maybe it's a stupid question, but can I use a voltage power supply (VLED) to feed my led array, of (let's say) 24V, or more, even though the max OUTx of the TLC is 17V (VLED>17V)?
In my setup, I have an array of 7(or 8 also) led in series, the led Vf is 3.2v. Thus, the total voltage drop (VDROP) is 22.4V.
As far as i can understand, since the OUTx of TLC59116 is in 0-17V with max 120mA, this means that the difference between the led power supply and the led voltage drop
has to be less than 17V, so VLED-VDROP <= 17V. It this true?
Another question related to this point is about the power dissipation calculation.
I cannot find any formula in the datasheet, I was thinking something like this
Ptot = (Vled-Vdrop)*Iout*N + Vcc*Icc
where N are the channel, Vcc and Icc are the maximum power supply and current for the TLC59116, respectively.
Can i assume a formula like this? Are there other factor i have to consider (i.e. i2c power, etc)?
My biggest concern is always about the relation between VLED, VDROP, and OUTx of the TLC.
Thank you,
nicola