This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Schematic check request

Part Number: BQ25792

Hello Sir:

Please help use check our schematic.

If there has any wrongs please let us know.

Looking forward your feedback.

Thanks a lot.

  • Hello,

    My schematic review is as follows:

    1. The 0.1 uF VBUS, VSYS, and PMID capacitor is recommended to be rated for 50 V on our EVM.

    2. The 4.7 uF REGN capacitor is recommended to be rated for 16 V on our EVM.

    3. I cannot see your input MUX, so I cannot verify that.

    4. D+ and D- configured for DCP.

    5. ILIM is correct for Vin above 5 V. Please note that REGN voltage changes slightly with input voltage which will affect this divider.

    6. 1.5 MHz 2s selection on PROG to match 1 uH inductor.

    Regards,

    Mike Emanuel