Other Parts Discussed in Thread: TPS2113, TPS631000
HI.
TPS61021A-PWR723 EK is being tested.
TPS61021A-PWR723 EK DATASHEET 2page is said to be possible up to 1A when VIN=1.2V/VOUT=3.3V
I changed EK R3 to make VOUT=3.9V and applied VIN=1.5V as a power supply. At this time, the load current is MAX400mA.
However, as shown in the attachment below, 1V DROP is periodically generated.
The same applies to adding CAP to C6.
The output current seems to be insufficient. Is 1A correct?
It seems to be less than 400mA.
BR.
KWON.