The min input voltage for the TPS76933 is stated at 4.3V. If 3.3V were to be supplied to the input, what will the output of the TPS76933 be, assuming 30mA load when the chip being driven by the LDO is ON?
Thanks for helping out!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What power specs (Vin range, Vout, Iout) do you need to meet? There is a power quick search at power.ti.com that can help you find the right part.
Also, you need to consider what minimum voltage your load requires. It won't be 3.300000V. It will likely be 3.3V +/- some %, such as 5-10 %. In this case, you could use an LDO since it meets your load's needs.
We also have buck-boost charge pumps and buck-boost switchers that will work for you.
Chris,
The problem here is that we already have an existing board http://focus.ti.com/docs/toolsw/folders/print/cc2540usb-rd.html which uses the TPS76933. For typical applications the board was going to be driven by USB where the supply voltage is greater than 3.3V, the LDO would work perfectly fine.
However, we have a customer who wants to know if they can use it with 3.3V without having to hack the board. Unfortunately since the supply voltage of 3.3V is less than the 3.4V min for this device to function, we wont be able to use the existing board for this supply application.
The device will still 'function' (be on) at 3.3V in. The issue is that Vout will be about 3.2V at a 50 mA load. You will need to see if your load can accept this lower voltage.
Ah yes!
The control will turn on the LDO MOS as hard as possible. There will be no voltage regulation, but the circuit will work. Thanks for settling this for me.