Other Parts Discussed in Thread: TPS54J061, TPS54JA20, TPS548A28, TPS543B20, TPS543820, TPS543A26
Hi,
we are choosing part TPS568215RNNR for our design having following requirements,
1) For 3.3V output
Vin = 5V
Iout = 2A (actual continuous load)
Total Capacitance load = 1175 uF (considering all decoupling capacitors)
2) For 1.8V output
Vin = 5V
Iout = 1A (actual continuous load)
Total Capacitance load = 120 uF (considering all decoupling capacitors)
3) For 1V output
Vin = 5V
Iout = 2A (actual continuous load)
Total Capacitance load = 120 uF (considering all decoupling capacitors)
We need following thing,
1) Whether selected buck converter is good to go.
2) Require EMI-EMC reports/graph for the same.
3) Any EMI filter to be added to make it EMI compliant.
4) In simulation (Webench), how to add capacitive load as per our need?
Thank you.