Hi,
We will use the LM5170 for the boost circuit, and we know LM5170 can support the 4-phase or 3-phase operation by SYNCOUT signal,
and we search the LM5170EVM-BIDIR can support the 48V-12V dual battery system applications, the 60-Adc MaximumMultiphase from or into the 12VDC-Port;
Now we want to know if this device can suppor the input voltage 24VDC(Compatible 12VDC system), the output voltage is 48V/60A design,
and please advise if we can design 3-phase or 4-phase to improve the load capacity, thanks.