This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3421: Query the Tolerance of the High

Part Number: TPS3421
Other Parts Discussed in Thread: PCA9534A,

I saw some of the datasheet like pca9534a indicates the tolerance of the High in the datasheet:

I can calculate the tolerance of high by this diagram. (tolerance = 1.0-0.8=0.2 (mm)).

But in the datasheet tps3421,there is only the max high.

 The datasheet only gives the maximum high; there is no information regarding the high tolerance.

Is there any information regarding the tolerance in high for this datasheet?

Or this datasheet's tolerance is not available.

Please advise If I am wrong.

Thank you.