Hi team,
Does UCC28056 support wave soldering?
If so, is there any problem with the following conditions?
-Maximum temperature: 255℃ or higher
-For 5 seconds
Best,
Ryu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Does UCC28056 support wave soldering?
If so, is there any problem with the following conditions?
-Maximum temperature: 255℃ or higher
-For 5 seconds
Best,
Ryu
Hi JCHK,
Thank you for your reply.
The document you gave us is the result of evaluation with 16-pin SOIC, but UCC28056 is a 6-pin SOT-23.
Is it correct to say from this document that there is no problem with all surface mount components under the conditions you evaluated?
Best,
Ryu.