Hi,
The register 0x25 is only for two phase application, it should not be
accessed in two channel application, right?
BTW, two phase application is only supported in CV setting, not in
CC setting, right?
Honda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The register 0x25 is only for two phase application, it should not be
accessed in two channel application, right?
BTW, two phase application is only supported in CV setting, not in
CC setting, right?
Honda
Hello,
1. Yes, Reg 0x25 is only used in two phase CV mode and is not needed for two separate channels operation.
2. Yes, two phase application is only in CV setting and not in CC setting.
Thanks Tuan