This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM340: TO-3 Package Pinout

Part Number: LM340

For the TO-3 package, on page 1 of the datasheet, it shows Pin1 as Input, Pin2 as Ground, and the case as Ground or Output, so case would be Output

On page 3, it shows the two pins as INPUT and OUTPUT and the case is GROUND

Which is correct?