This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25155EVM: Using USB2Any with BQStudio

Part Number: BQ25155EVM
Other Parts Discussed in Thread: BQSTUDIO, USB2ANY, , EV2400, BQ25790

Can the USB2Any be used with BQStudio? I have the USB2ANY from a previous evaluation board. I'm testing with the BQ25155EVM, but it only seems to work with the BQStudio and EV2400.

  • Hi Jeff,

    Unfortunately the BQStudio software is only designed to work with the EV2400. The USB2ANY can be used to communicate with this charger but in a much more manual way. The TI Charger GUI allows for manual use of the I2C bus via the command sequence page. You can select the BQ25790 on the TI Charger GUI page, select the paper icon on the left hand side, and manually configure the I2C transactions to execute.

    Best Regards,

    Juan Ospina