This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62065-Q1: Current detection and temperature detection

Part Number: TPS62065-Q1

Hi team,

could you help on the following questions:

  • Time required for current/temperature detection,( this is the time from the temperature (current) anomaly to the shutdown of the output )
  • Whether the test is determined by multiple tests or is closed as soon as a peak reaches?
  • Recovery time,Recovery time, the time from when the chip detects that the temperature (current) returns to the normal range to the normal voltage output

thanks