Hello,
How much does a TPS546D24A draw a current from its AVIN pin when the converter is in switching operation? I'd like to have a plot of the AVIN pin current over switching frequencies if it's available. If not, could you provide me with the IAVIN value under the following conditions?
- Input voltage: 12 V
- Switching frequency: 650 kHz
- Output voltage: 0.4 V to 0.7 V
- Output current: 28 A
Best regards,
Shinichi Yokota