Hello,
I am confused about the threshold limits (min/max values) of Precision window supervisor IC TPS3850G33DRC, which has been used for OV & UV monitoring in one of our existing board. As per datasheet nominal thresholds are mentioned as a percent of the nominal monitored voltage which are, VIT+(OV) = 4%; VIT–(UV) = –4% of 3.3V (nominal monitored voltage option in our case which is going to the SENSE input).
if my power supply tolerance is from, 3.207V (min.) - 3.3V (typ.) - 3.472V (max.) then will the TPS3850 thresholds vary accordingly for overvoltage? for e.g. if in one of the scenarios my power supply is maximum (3.472V) then will the threshold values of TPS3850 be ±4% of 3.472V (max. value)?
Thanking you in advance.