This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck Boost regulator selection.

Other Parts Discussed in Thread: LM5175, LM5176, TPS55288

Hello There,

We are designing a new product for automotive applications (like ECUs) that is powered by an input source of 9 to 36 V, and the ambient temperature of 65 degrees Celsius. we need a few regulators for that, which are listed below.

Regulator1: Output = 12 V 5 A; Regulator 2: Output = 5 V 10 A; Regulator 3: 5 V 15 A. We found the LM5175 series 4-switch buck boost converter to be suitable for our application. in that we have a few questions.

The problem with the LM5175 is that it requires more space; our board does not have that much space, hence we need a smaller buck boost controller, so can you please list the available buck boost regulators to satisfy all our needs?

Thanks,
Sakthivel