This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54231 UVLO

Other Parts Discussed in Thread: TPS54231

Hi,

 

Please can anybody help me with my below query.

I dont want to use external UVLO option by providing pullup and pull down resistor to enable pin. 

Vin for the regulator is fixed 12V and Vout is 1.2V.

As per datasheet of TPS 54231 "It is recommended to use an external VIN UVLO to add Hysteresis unless VIN is greater than (VOUT + 2 V)".

In my design Vin > Vout+2V and for my design Internal under voltage lockout threshold of 3.5V is good enough(as per datasheet). 

so do I really require to use external resistor for UVLO?

I want to enable the regulator by connecting the enable pin to open drain output signal.

Please help me to understand, if there will be any problem in enabling the regulator with open drain output signal without the external UVLO resistor?