This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5024: Question about Max_Current_Option setting

Part Number: LP5024


Hello,

My customer plans to use LP5024 at the following conditions.

Vcc=3.3V

RIREF=7.35Kohms (ISET=10mA)

In this case, which value should Max_Current_Option bit be set, 1 or 0?
Or, ISET =10mA is much smaller than either IMAX 25.5mA or 35mA, Max_Current_Option bit can be 1 or 0?

Best regards,

K.Hirano