Hi Team,
We are using Power cube v3 which is capable of providing three output voltage (Output 1: 5V, Output 2: 3.3V, Output3: 12V)
Image for reference
where LM5116 buck controller and mosfet BUK6226-75C is used in the design.
When we are giving the input supply(48V@2200mA) with battery,12V output is not coming up and we found that both HO,LO mosfet going short.
We are still getting output 1: 5V, the 5V rail looks fine but output 3:12V rail we are facing this issue.
We tried changing the mosfet again we faced the same issue: output 3:12V not coming up, short in mosfet.
For these above cases are tried without connecting any load.
So, what causes the mosfet gone bad and affecting the 12V output rail?
Waiting for the response.
Regards,
Sathya Priya N.