This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546D24A: IOUT_OC_FAULT_LIMIT by MSEL2 Resistor

Part Number: TPS546D24A

Hello,

In Table 7-11 of TPS546D24A's data sheet, the Register-To-AGND Code value from 4 to 7 sets 39 A to IOUT_OC_FAULT_LIMIT command. However, I guess the set value of 39 A is not effective and will actually be rounded up to 40 A because of the limitation of the TPS546D24A's analog hardware described in the section 7.6.39 (46h) IOUT_OC_FAULT_LIMIT.

Is my understanding correct?

Best regards,
Shinichi Yokota