Hello. I have a question regarding the TPS2H000B. It is suitable for 24V automotive applications? My main concern is the 36V due to short-to-battery event, another can be load dump etc. Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. I have a question regarding the TPS2H000B. It is suitable for 24V automotive applications? My main concern is the 36V due to short-to-battery event, another can be load dump etc. Thank you!
Alex-Cosmin,
The TPS2H000B-Q1 is made for 12V automotive systems and therefore would not be guaranteed to handle 24V transients such as load dump. We do have devices in the roadmap (short-term and long-term) for 24V systems, however would it be OK to follow-up with you via the email on file to share details?
Best Regards,
Tim
Yes, I would appreciate if we could continue through e-mail with more details about 24V devices.
Thank you!
Alex