This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: The output current after hard short and soft short occurs is less than the minimum value of ILIM

Part Number: TPS2595


Dear Specialists,

My customer is evaluating TPS259540 and has a question.

I would be grateful if you could advise.

---

The output current after hard short and soft short occurs is less than the minimum value of ILIM

Could you please let us  know the reason for this kind of behavior.

(1)When a soft short circuit occurs, the output voltage drops to 0V, but the output current is keep flowing approximately 300mA.
According to the datasheet it should be 0A.

(2)When a hard short occurs, the output voltage drops to 0V, but the output current flows constantly 300mA.
It should be 0A in the datasheet.

---

I'd like to send the customer's schematic and waveform, could you please provide a friend ship or e-mail address. 

I appreciate your great help in advance.

Best regards,

Shinichi