Hi Sir,
My customer is asking some questions about LM76005-Q1.
He would like to use the design condition V-in = 4.5~60V (normal case is 9~36V), V-out = 4.2V, I-out = 5A.
Since the webench tool could not simulate this design condition. May I know if the design condition is OK?
In the worst case, when the V-in drops to 4.5V about 100ms(same as the 12V system on the test item 4.6.1 of ISO16750-2 standard), may I know if the system keeps working normally? ( V-out = 4.2V and I-out = 5A)