I have designed a board using the TPS61196 6 string 400mA WLED driver and copied the circuit from the TPS61196 EVM board. We have checked the board for all continuity and are seeing the expected values with no fault at all of the pins other than the Switching Frequency for the MOSFET Q1 and the board fails to boost the input.
I have substituted our designed board for the evaluation module and the TPS61196EVM functions properly. Once the designed cirucuit is substituted for the TPS61196EVM our circuit does not function. We have replaced the TPS61196 driver on the board and followed the schematic of the evaluation module one to one and were hoping that we could receive support from TI in debugging this issue.
I have attached a schematic of the designed board in-use and I am generally available from 7AM to 4PM EST for any further questions or communications