This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC DC Conversion

Hi,

Can any one help on best architecture to generate multiple voltages typ like 1.2V@6A, 1.8V@4A, 2.5V@4A 3.3V@4A from single 12V input

Best Architecture like

Case 1.SWR>>>LDO's

Case2.SWR>>SWR

etc...

Any other efficient configuration?.

SWR: Switching Regulators:

LDO: Low Drop Out

Regards,

Murali R

  • Hello Murali,

    We do not have a wide VIN PMIC that will be able to supply those currents at those voltages.

    Best Architecture like

    Case 1.SWR>>>LDO's

    Case2.SWR>>SWR

    etc...

    Now when speaking on these architectures, are you speaking on having a SWR before a PMIC, we may have a solution like that available.

    What is the target application for these voltages, safety application SoC or an industrial SoC?

    BR,

    Nicholas