Other Parts Discussed in Thread: BQSTUDIO,
The customer encounter some issues when OTP in their lab when using BQstudio.
1. When entering the CONFIG_UPDATE mode, whether we could write the register value into RAM? Because after entering CONFIG_UPDATE mode, when I click write all, there always be communication failure.
2. In the step 5, if not in the config_update mode, the BQ76942 will trigger CUV(Cell under voltage protection). And then BQ76942 will enter shutdown mode. Is there any solution for this?
3. When using OTP function in BQstuido as below, do we still need to enter CONFIG_UPDATE mode manually? Or the Program OTP have included the enter-CONFIG_UPDATE-mode command?
4. Now the customer are using Program OTP directly without sending entering CONFIG UPDATE command. Besides, the customer are shorting TS2 to GND when OTP, so that the BQ76942 will not enter Shutdown mode. Is it a useful way? In the actual usage, there are some possibility could OTP successfully.