This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suitable regulators for LCD backlight

Other Parts Discussed in Thread: TPS92381, TPS923652

Hello, we are designing a new product that must provide power to an LCD display, 100mA at 18 or 19 V DC for the back-light diodes.

I have searched through the datasheets, the TPS92381 seems suitable, but there are many others, so would like to ask for guidance.

The IC must be integrated with a mixed analog and digital MCU board, so it must produce very little EMI.

Market is cost sensitive, so it must be economical.

Average current at 18/19V DC to the backlight diodes is 60 mA.

Operational temperature range ideally should be -10 to 85 celcius.

IC must be be available for the next 5 years.

Appreciate guidance. Thanks