This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2664: LM2664M6X/NOPB

Part Number: LM2664

Hi,

I have been using LM2664M6X/NOPB for one of my projects.

Design Requirement:

Input Voltage: 2.5V

Output Voltage: -2.5V

Output Current: 40mA

Components:

C27: 2.2uF, 10V

C28: 3.3uF, 10V

C38: 3.3uF, 10V

Please review the below attached design and drop your comments.