Hi,
For the circuit similar to the one mentioned in the datasheet of TPS563257, I have connected 47k and 20k resistor (10nF is not connected) for the voltage divider to the enable pin.
The supply voltage is steady 5V DC, the voltage divider is supposed to deliver 1.49V to the enable pin.
When not connected to enable pin (pin number 5), the voltage divider works just fine,
but as soon as the voltage divider is connected to the enable pin, it only delivers negligible volts, i.e. around 250mV.
What could be the possibility for the failure?
Please consider Figure 8-1 from datasheet of TPS563257DRLR