Hello,
I am using LM5035 IC for my half bridge configuration. The input voltage is 270VDC. Hence, I am supplying VIN to IC by and external 12V supply.
I have few queries:
1.How I can achieve UVLO, RAMP, OVP pin voltage if the grounds are different for IC supply (VIN --12V) and Source Voltage (270VDC). Also need to provide gate isolation using gate drive transformer.
2. How I can obtain differential output voltage using same half bridge topology.
3. If I am using diode at secondary side, then what to do SR1 and SR2 pins. (floating or gnd)