This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

charge pump

Other Parts Discussed in Thread: LM2660

Hi Team, 

just want to check if there is p2p SOIC-8 charge pump 

actual application: +5V to -5V or +12V to -5V 

requirement : 3-18V Vin, -3~-18V Vout, 100mA.  Fsw= 120k~1.25MHz, 

I checked the website and seems no 12V Vin charge pump, then only +5V Vin. please kindly help recommend suitable one. Thanks. 

BRs

Given