This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74502Q1EVM: Implementing LM74502Q1 for 5V @ 2A input

Part Number: LM74502Q1EVM

Hi team!

I looking to use LM74502Q1 for a 5V @ 2A input, with over voltage protection of 5.5V, under voltage of 4.5 and reverse polarity.

My first question: Which part is more suited for this application, LM74502-Q1 or LM74502H-Q1?

My second question: Can I use LM74502Q1EVM to try this application by changing the resistors on it by the following formula:


Thanks,

Moral.