Part Number: BQ25890
Dear experts:
If the input voltage VBUS stays below DPM threshold for a while. REG13 IDPM_LIM will fall down to minimum value 100mA. When the input voltage ramps up again. Sometimes we can find "Maximum Input Current Detected" in REG14 bit 6.
When it happened, IDPM_LIM would be locked at 100mA, unless the battery is depleted, or we issue a system reset.
Anyway, we duplicate this problem by using power supply. Maybe the ramp-up speed is too fast. I just want to confirm, this scenario is correct. IDPM_LIM will be locked at 100mA after "Maximum Input Current Detected".
Thanks for replying!