Hi Team,
Could you please help share the date of min regulation limit of IINDPM at 2.5/2.6/2.7/2.8/2.9/3.0A?
Best Regards,
Jaden Yue
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jaden,
Unfortunately we do not have data to share on the min regulation limit for the values requested because we do not provide a min and max spec for every possible value IINDPM can be set to.
The general principle will be the same for IINDPM = 2.5/2.6/2.7/2.8/2.9/3.0A as it is for the lower settings shown. For example 2.5A setting max is 2.5A and for 3A setting max is 3A. Since we do not provide a spec in the EC table for the IINDPM values requested I am unable to provide a precise minimum value.
With that in mind the minimum value is expected to be roughly in the range of -10% to -15% below the set value, but this is not guaranteed.
Best Regards,
Garrett