This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02013: Why single phase PFC output is kept at 400V

Part Number: TIDM-02013


Hello experts,

Why most of the single phase pFC output is kept at 400V ?

is it because of any kind standards limiting Single phase PFC out at 400V ?

Incase of any kind of requirement demands more output voltage, it can be achieved by using single phase PFC itself ? only by changing the Set value of the voltage in firmware.

Thanks and regards

Anoop kumar N