Other Parts Discussed in Thread: TPS922053
Hello,
Could you elaborate on the TPS92513 5% LED current accuracy specification please?
Let's say my full scale current is 500mA and a DC voltage is used for dimming. Am i to expect 475mA - 525mA output due to the accuracy at this full scale current?
I then use the dimming input to set the current to 10% of full scale, 50mA, can I expect the 5% still hold to give me a range of 48mA to 53mA, or will it be in the range of 25mA to 75mA (+-5% of full scale current)?
Thank you!